LifeCheck with hand-held testing devices

Functional monitoring of the arrester is possible with all protective devices marked with the LifeCheck symbol.

With the practical hand-held testing device, you can soon find out if your protective components have suffered damage due to electrical or thermal loads. This keeps you in the picture and allows you to exchange overloaded protective modules in good time.

This is the test procedure

The LifeCheck symbol can be found on the arrester module

Version 1 - The arrester module remains plugged in

If the installation is equipped with arresters of this type only, the arrester module can remain plugged into the base part during testing.

Version 2 - The arrester module is pulled out

If the installation is equipped with arresters of this type or a mixture of different arresters, you need to pull the arrester module about 5 cm out of the base part.

Your advantages with version 2:

  • It is clear to which arrester module the test result applies
  • It is immediately recognisable which arrester is being tested (even if you have to interrupt the testing procedure)
  • When using the universal base part BXT BAS as a feed-through terminal, the signal is still available when the arrester module is taken out.

Step by step procedure - version 2

LifeCheck Prüfablauf
Test procedure LifeCheck - 5 Steps
  1. Clip the test sensor onto the arrester module
  2. Pull the arrester module out by about 5 cm
  3. Start the test and wait for the result
  4. Plug the module back into the base part - you must hear it click in
  5. Finished. Remove the test sensor from the arrester module and follow the same procedure with the next arrester
Contact

Have you got any questions? Contact us.

Technical support

Phone: +49 9181 906 1750

back to top