The power of energy industry lightning protection
Preserve your power quality with DEHN today
According to the U.S. Department of Energy’s (DOE) 2023 U.S. Energy and Employment Report (USEER), the energy sector was one of the top job markets in terms of growth, highlighting increasing demands for the industry’s services.
Without your energy supply operation, much of the U.S. would be without reliable power. So why would you risk your critical facilities and operations by leaving them vulnerable to transient voltage threats such as a lightning strike or internal system surge?
NEC and other industry regulations haven’t kept up with the growing threats to your systems, but that doesn’t mean you have to fall behind as well. Invest in the protection you need to minimize power quality disturbances and safeguard your service.
DEHN is a global electrical engineering company. We have the solutions you need in order to learn about the risks to your systems and eliminate them before the worst-case scenario occurs.
Contact our industry-leading transient voltage experts today.
Request a risk assessment![](/sites/default/files/styles/1_1_ratio_400_x_400/public/media/images/2021-02/portlet_-_stromerzeugung.jpg?h=21b1a8e3&itok=2Me-iMao)
The shocking reality of transient voltage threats to energy supply systems
Transient voltage is an ever-present threat to the safety and success of your organization and operations.
External transients, such as lightning strikes, are becoming increasingly more common as climate change breeds more frequent extreme weather events. However internal risks stemming from the daily electrical noise of your own internal systems still make up about 80% of transient-related power quality disruptions.
As a main player in the energy supply industry, your impact stretches far beyond your own systems and facilities into the power grid and the homes and businesses of the customers you serve. If your electrical systems aren’t properly protected, you may not be able to successfully manage this great responsibility.
When the overvoltage resulting from a transient electrical event occurs, it can damage your facilities and systems, as well as threaten the safety of your employees. In more extreme cases, the damage could cause total power failure and grid instability that inhibits your ability to fulfill contractual obligations and meet your growth and service goals.
Talk to DEHN to learn about the specific risks facing your company and get proven solutions before it’s too late. Request a risk assessment today.
Supplying surge safeguards to diverse energy sectors
As an international transient voltage protection powerhouse, DEHN has experience in all sizes and scopes of markets. Within the energy supply industry, we’ve tailored our innovative solutions to the individual needs of several specific sectors, including:
- Solar energy
- Biogas plants
- Power grids
- Wind energy
Request a risk assessment today and get in the know about the threats to your unique energy supply business.
Transient voltage protection to ensure solar success
Solar systems and photovoltaic systems are critical infrastructures within the energy supply industry. PV systems specifically are at the top of global energy source lists and have a large role in the production of reliable energy for North American consumers.
As PV and solar systems are often housed outside in designated open fields or on rooftops, they are exposed to harsh elements including weather-related external transient voltage threats. Additionally, their wide distribution makes them and their connected systems more susceptible to electrical events if left ungrounded.
While these systems are designed to withstand diverse weather conditions, surges resulting from a lightning strike can penetrate their basic factory defenses and compromise the extremely vulnerable electric components inside. Even the smallest malfunction can lead to a chain reaction that can disrupt the power quality of the entire PV plant and the connected power grid.
Though lightning protection systems should be a top priority for solar systems, the most effective power quality protection for any energy supply sector consists of grounding systems, as well as both internal and external protective solutions.
DEHN specializes in solutions for the following PV and solar systems:
Rooftop PV systems
While the installation of a PV system on top of a building or energy supply facility does not necessarily increase the risk of lightning strikes, its direct connection to the building’s electrical infrastructure can make the effects of lightning-related overvoltage more severe.
DEHN has the knowledge and expertise necessary to implement protective solutions for PV systems on rooftops that observe separation distance standards and account for various system configurations.
Free-field systems and solar parks
Lighting protection systems for solar parks can protect the entire power plant area from lightning-related damage, as well as safeguard modules, inverters, and monitoring systems from transient electromagnetic impulses and the resulting overvoltage.
Our solutions accommodate a variety of possible options, including a centralized configuration with a central inverted or a distributed configuration with a string inverter.
Request an assessment with DEHN today.Electrical threats that impact biogas plants
It's especially important to minimize power quality disturbances to biogas plants as they house and work with a plethora of toxic, flammable, and downright dangerous chemicals and pharmaceutical products.
Even a small electrical disturbance could trigger detrimental damage throughout all aspects of your plant, compromising your electrical systems and your ability to safely manage these hazardous materials. As a result, your energy supply company could face harsh legal penalties and financial repercussions related to production downtime, costly repairs, and non-compliance with environmental standards.
One of the silent heroes of the biogas sector is storage facilities and tanks. When you’re not using your chemical products or are in between processes, you need a safe place to house these materials. Without proper transient voltage and lightning surge protection, these important facilities are exposed to serious threats. The sites and natural environment around them face fires, explosions, and chemical spills caused by lightning strikes or internal transient surges.
As part of our comprehensive transient voltage protection solutions, DEHN offers fire protection and explosion prevention systems for these high-risk environments within biogas plants. We’re experienced in everything from protection devices that minimize the risk of fires igniting after a lightning strike to surge protection devices that monitor and maintain fire fighting and cooling systems.
Contact DEHN today to be informed of the risks to your biogas plant.Power grid protection to fight the blackout blues
The U.S. electric grid is a large network of power plants, power lines, and distribution centers that work together to provide reliable electric power. While the power grid is one of the largest cohesive infrastructures in the country, it often goes unnoticed by the general public, working behind the scenes to power industrial facilities as well as households.
Attention typically only shifts to the grid when a major electrical event or weather phenomenon affects grid stability in a significant way. The large-scale blackouts caused by unusually harsh winter weather conditions in Texas in 2021 sparked widespread discussion about the setup and reliability of our grid and power quality.
As climate change continues to progress and new threats, such as cyberattacks, loom higher over the stability of the electrical grid, it’s more important than ever to pursue proactive protection from these external and internal electrical events.
The good news is that DEHN is a partner who knows the risks and understands how transient voltage will affect your operations. We can help implement solutions that will reduce the need for expensive maintenance and repair work and maintain your power quality as an important part of the U.S. electrical grid network.
Our solutions extend to every aspect of your grid systems, including electric battery storage systems to help counterbalance fluctuations and peak loads from electrical components in the energy supply sector. Surge is a natural part of the power grid, but without protection, it could render your sensitive systems, like battery storage centers, inoperable.
Contact DEHN to get started on a tailored protection concept.The sky-high costs of surge-related damage to wind energy
While much of the power grid is still relying on fossil fuels to power the country’s electrical systems, many leaders in the energy sector are turning to renewable energy sources such as wind energy.
In fact, more than 70,000 wind turbines work to create clean reliable electric power across the U.S. according to the American Clean Power Association. Like solar systems, these powerful giants are exposed to the elements and their locations’ weather conditions, opening them up to more frequent and extreme external transient surge threats.
A lightning bolt that makes contact with a turbine can cause significant damage to rotor blades, bearings, and internal components in one split-second strike. Not only is this damage extremely costly to address, but any resulting downtime or system-wide overvoltage could disrupt service and compromise your contracts.
Transient voltage threats change with the wind, but the risks to your wind energy systems don’t have to be finite. With proactive action, such as requesting a risk assessment from DEHN, you can take the first step to combating power quality disruptions before they strike.
Reach out to DEHN to start your journey to proper protection today.Proven solutions to keep the lights on
DEHN Inc. has worked in the energy supply industry in North America for more than 20 years. As electrical threats change and evolve, so do our solutions, resulting in our detailed, all-encompassing approach to protection that keeps your systems running even in the face of daily surges or indirect lightning strikes.
While our Red/Line surge arresters tackle power quality issues within your sensitive electrical components, our Yellow/Line lightning arresters and surge protection devices safeguard signal stability and communication lines. All our solutions are compliant with industry standards and regulations including the National Fire Protection Association (NFPA) 780.
Our products tailored for energy supply applications include:
- BLITZDUCTOR XT
- Pipe clamp for explosion hazard areas
- DEHNguard
- Air-termination systems
The most effective lightning protection systems combine internal and external solutions for a complete package that addresses the full spectrum of transient voltage issues.
Our process is simple. First, request a risk assessment, and our experts will get you up to speed on everything you need to know about the threats and opportunities for your distinct systems and facilities.
Get in touch with us today to identify the right products and services for your energy supply operation.
Request your risk assessment today![](https://www.dehn-international.com/thumbor/unsafe/fit-in/640x360/filters:fill(ffffff,false)/www.dehn-international.com/store/f/46644564/HDVORSCHAU/920310.jpg)
920310
Lightning current arrester module 4-pole BLITZDUCTOR XT with LifeCheck
Space-saving four-pole lightning current arrester module with LifeCheck feature for almost all types of applications.
![](https://www.dehn-international.com/thumbor/unsafe/fit-in/640x360/filters:fill(ffffff,false)/www.dehn-international.com/store/f/45808367/HDVORSCHAU/920381.jpg)
920381
Surge arrester module for two pairs BLITZDUCTOR XT Ex(i) with LifeCheck
Space-saving LifeCheck-equipped surge arrester module for protecting two pairs in intrinsically safe measuring circuits and bus systems. feature for almost all types of applications.
![](https://www.dehn-international.com/thumbor/unsafe/fit-in/640x360/filters:fill(ffffff,false)/www.dehn-international.com/store/f/43813377/HDVORSCHAU/540821.jpg)
540821
Pipe clamp f. hazardous areas D 6-27mm with terminal screw M8 Ms/gal Sn-StSt
Pipe clamp for hazardous areas, for electrical contacting of pipes in hazardous areas.
Work with DEHN – Request an assessment
At DEHN, we understand that when it comes to your energy supply operation, you're the expert. That's why we believe in a collaborative approach every step of the way, from conceptualization of a lightning protection system to execution. Our team will tailor solutions to precisely fit your unique requirements for your delicate photovoltaic systems, wind turbines, and biogas plants.
With more than a century of expertise under our belt, we're excited to deliver transient voltage and lightning protection solutions that have a lasting impact on your power generation and power systems. Reach out to DEHN today and request a risk assessment to safeguard your electrical future.
Request your risk assessment