DEHNshort protects the waterpark
Freizeitbad Stegermatt
Freizeitbad Stegermatt
It was already clear during the planning of the waterpark that arc fault protection would play an important role in terms of system availability and the protection of people.

DEHN solution | Tested protection concept against arc faults |
Customer | Freizeitbad Stegermatt |
Project | Electrical engineering planning |
Sector | Leisure and relaxation |
Location | Offenburg |
Planning | Planungsbüro Alexander Müller GmbH |
Product | DEHNshort |
The challenge
Availability is the top priority for a public swimming pool like the Stegermatt waterpark. A short-circuit-related failure of the power supply could result in the pool being closed for up to 4 weeks. This would be difficult to communicate to the public and would mean huge damage to the operator's image.
The technical operations of the city of Offenburg were convinced of the advantages of an arc fault protection system.
The solution
With the DEHNshort arc fault protection system, Freizeitbad Stegermatt has laid an important building block for system availability.
The investment is low in relation to the total volume, and the main distribution board, an important artery of the waterpark, is now permanently protected against outages caused by arc faults.
DEHNshort enables the affected switchgear to be put back into service quickly. This means shorter downtimes and lower follow-up costs.

DEHNshort in Freizeitbad Stegermatt
Klaus Bastian says:
"Closing the waterpark due to a power supply failure would be a huge blow to the operator's image."
Klaus Bastian
Project Manager at Planungsbüro Alexander Müller GmbH,
in charge of electrical engineering planning for Freizeitbad Stegermatt in Offenburg
Interview with Klaus Bastian
Planner? Want to protect your system from arc faults?
Simply send a mail to our technical support or call us on: +49 9181 1750.
We will be happy to return your call and respond to your queries in detail.